Connect Remotely
You can connect to a AKD PDMM or PCMM from an external network using VPN or other tunneling protocol. To do so you must open the following ports which are used by KAS to connect to a controller.
| Port | Component/Protocol using the port |
|---|---|
| 80 | KAS IDE |
| 502 | HMI and other Modbus devices to communicate with Modbus TCP. |
| 2222 | Ethernet/IP communication |
| 4002 | KAS IDE: Oscilloscope variable monitoring. |
| 4003 | KAS IDE: Communication with the PLC |
| 9900 | KAS IDE: Communication with the runtime engine; WorkBenchviews. This is necessary for the connection to the runtime. |
| 34962 | Profinet communication |
| 34964 | Profinet communication |
| 44848 | Ethernet/IP communication |