Overview: Create Variables
Variables may be created in either of two ways:
- From the Variables tab of the Dictionary. Clicking Add Variable opens the Create Variable dialog box.


- From the program Editor. Below we see examples of the FBD
"Function block diagram"
A function block diagram describes a function between input variables and output variables. A function is described as a set of elementary blocks (click on the Variable button) and FFLD (double-click on the in or out pins of the function) Editors. Enter a name and click OK to open a dialog box that allows you to define the variable.