Using the AKD PDMM or PCMM Controller
Tasks related to the controllers are:
- Configure parameters
- Start and stop your KAS application
- Update the firmware
- Reset to factory settings
Rebooting the controller, recovering the firmware, and resetting the controller may be performed from the device or, more conveniently, using the web server.
-
-
Please note that any reference to AKD PDMM or PCMM refers to both the 800MHz and the single- and dual-core 1.2GHz variants, unless otherwise noted.