ACTION.RUNNING

Description

This keyword displays which tasks are triggered in the current cycle. Each bit is for one task, bit 0 is for ACTION1, bit 1 is for ACTION2, etc. For continuous tasks, the bit is 1 for each cycle the task runs, and 0 for each cycle the task does not run. For edge-triggered tasks, the bit is 1 for cycles where the task is triggered, and 0 otherwise.

Examples

Code

--> ACTION1.ACTIVE 1
--> ACTION2.ACTIVE 1
--> ACTION.RUNNING
0  

Context

See Actions Table.

Versions

Action Version Notes
Implemented 02-00-03-000

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

0

Data Type

Integer

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.