ACTION#.ACTIVE
Description
Sets whether an action is disabled or enabled. When set to 1, the action will be executed if it is valid.
| Value | Description |
|---|---|
| 0 | Action disabled |
| 1 | Action enabled |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported