ACTION#.RUNCOUNT

Description

This keyword displays the number of times an action ran since the time the Action was activated. It does not take any arguments. When an Action is activated, it automatically clears this count. The count value is only available for edge-triggered tasks and not for continuous tasks.

Examples

Code

--> ACTION1.ACTIVE 1
--> ACTION1.RUNCOUNT
0  

Context

See Actions Table.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

0

Data Type

Integer

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.