AIN#.ZERO
Description
AIN#.ZERO causes the drive to zero the analog input signal (AIN#.VALUE). You may need to execute this command more than once to achieve zero offset.
-
- AIN#.OFFSET is modified in this process.
Examples
Code
--> AIN1.VALUE 0.056 V --> AIN1.OFFSET 0 V --> AIN1.ZERO --> AIN1.VALUE 0.000 V --> AIN1.OFFSET -0.056 V
Context
For more information see Analog Input.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Command |
| Units | N/A |
| Range | N/A |
| Default Value | N/A |
| Data Type | N/A |
| See Also | |
| Stored in Non Volatile Memory | No |
Variants Supported
All variants are supported.