AOUT#.CUTOFF

Description

AOUT#.CUTOFF sets the cutoff frequency in Hz for a single-pole low-pass
filter on the Analog Output.

A value of 0 Hz will turn off the filter and will allow all frequencies to pass through.

The filter can be used with all modes of Analog Output.

Examples

Context

For more information see Analog Output.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units Hz
Range 0 to 10,000 Hz
Default Value 0 Hz
Data Type Float
See Also  
Stored in Non Volatile Memory Yes

Variants Supported

All variants are supported.