AXIS#.CANOPEN.GEARPRIMARY.MOTORREV
Description
This keyword provides the count of motor shaft revolutions for the primary position gearing ratio calculation. It is part of the scaling calculation used for CANOpen
CANopen is a communication protocol and device profile specification for embedded systems used in automation for fieldbuses working in real time objects.
Context
See Scaling.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
1 to 4294967295 |
|
Default Value |
1 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
CANBus and EtherCat
Fieldbus Information
|
CANopen |
|
|
Index |
6091h |
|
Subindex |
1 |
|
Data Type |
U32 |
|
Float Scale |
1:1 |
|
Access |
Read/Write |
| PDO Map | No |