AXIS#.HOME.V
Description
AXIS#.HOME.V is the velocity used while homing. When searching for an index this speed is reduced by AXIS#.HOME.CREEPFACTOR.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
This content is not applicable to KAS.
Type |
Read/Write |
Units |
Rotary: RPM See Velocity Units for details. |
Range |
Depends on units. See Velocity Range for details. |
Default Value |
60 RPM Depends on units. See Velocity Units for details. |
Data Type |
Float |
See Also |
N/A |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Related Topics
Homing