AXIS#.IL.DIFOLD
Description
AXIS#.IL
"Instruction list"
This is a low-level language and resembles assembly.DIFOLD is the output of the drive foldback algorithm. It is an artificial current which is always above the drive continuous current, AXIS#.ICONT
. When AXIS#.IL.DIFOLD is lower than AXIS#.IPEAK, it becomes the active current limit.
AXIS#.IL.DIFOLD decreases when the actual current is higher than drive continuous current and increases (up to a certain level) when the actual current is lower than drive continuous current.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
Arms |
|
Range |
0 to 2,147,483.647 Arms |
|
Default Value |
N/A |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.IL.DIFOLD | 0x500A | 0x7 | DINT | 1000:1 | - | RO | False |
| AXIS2.IL.DIFOLD | 0x510A | 0x7 | DINT | 1000:1 | - | RO | False |