AXIS#.IL.FBSOURCE
Description
This parameter selects the feedback source that current loop uses for commutation angle calculation.
Feedback Sources/Connectors:
1 selects FB1 (connector X1)
2 selects FB2 (connector X2)
3 selects FB3 (connector X23)
4 selects FB4 (connector X21)
5 selects FB5 (connector X22)
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
1 to 5 |
|
Default Value |
1 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.IL |
0x500A | 0x6 | USINT | - | - | RW | False |
| AXIS2.IL.FBSOURCE | 0x510A | 0x6 | USINT | - | - | RW | False |