AXIS#.IL.KP

Description

AXIS#.ILClosed"Instruction list" This is a low-level language and resembles assembly.KP is used to read the proportional gain of the PI-loop that controls the q-component of the current.

The value is Read-Only, and is changed by modifying the current loop bandwidthClosedIn computer networking, bandwidth often refers to a data rate measured in bits/s, for example, network throughput. The reason for the connection of data rate with the term bandwidth is that the limit to the data rate of a physical communication link is related to its bandwidth in hertz setting (AXIS#.IL.BW).

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

V/A

Range

0 to 2,000 V/A

Default Value

N/A

Data Type

Float

See Also

N/A

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.IL.KP 0x500A 0x2 UDINT 1000:1 - RO False
AXIS2.IL.KP 0x510A 0x2 UDINT 1000:1 - RO False