AXIS#.MT.VCMD
Description
AXIS#.MT.VCMD returns the derivative of the position loop trajectory (AXIS#.PL.CMD), which is therefore a velocity. AXIS#.MT.VCMD is updated while the drive is in AXIS#.OPMODE 2 and is processing the following motion types:
- Motion tasking
- Homing
The Homing procedure allows, based on a position measurement, to set a position offset to the motor in order to ensure it is physically at the home position
- Electronic gearing
- Service motion
- External trajectory coming from a fieldbus
- External trajectory calculated from an analog input signal
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
This content is not applicable to KAS.
|
Type |
Read Only |
|
Units |
Rotary: RPM See Velocity Units for details. |
|
Range |
Depends on units. See Velocity Range for details. |
|
Default Value |
Depends on units. See Velocity Units for details. |
|
Data Type |
Float |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Related Topics
Motion Tasks