AXIS#.PL.OFFSET
Description
This parameter sets an offset that is applied to AXIS#.PL.FB.
Examples
The position feedback is at 1000 [deg]. AXIS#.PL.OFFSET is set to 500. The new position feedback is 1500 [deg].
-->AXIS1.PL.FB
1000.000 [deg]
-->AXIS1.PL.OFFSET 500
-->AXIS1.PL.FB
1500.000 [deg]
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-01-04-000 |
General Information
| Type | Read/Write |
| Units |
Rotary: counts, rad, deg, custom units, 16-bit counts Linear: counts, mm, µm, custom units, 16-bit counts See Position Units for details. |
| Range | Depends on units. See Position Range for details. |
| Default Value |
0 counts Note: Default is adjusted to account for the units selected by the user. |
| Data Type | Float |
| See Also | |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.