AXIS#.UNIT.ACCLINEAR

Description

AXIS#.UNIT.ACCLINEAR sets the units type for the acceleration and deceleration parameters when the motor type (AXIS#.MOTOR.TYPE ) is linear.

Type

Description

0

counts/s2

1

mm/s2

2

µm/s2

3

Custom Units/s2

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 3

Default Value

1

Data Type

Integer

See Also

AXIS#.MOTOR.TYPE

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.UNIT.ACCLINEAR 0x5010 0x6 USINT - - RW False
AXIS2.UNIT.ACCLINEAR 0x5110 0x6 USINT - - RW False