AXIS#.UNIT.PLINEAR
Description
AXIS#.UNIT.PLINEAR sets the units type for the position parameters when the motor type (AXIS#.MOTOR.TYPE) is linear.
|
Type |
Description |
|---|---|
|
0 |
counts |
|
1 |
Millimeters (mm) |
|
2 |
Micrometers (µm) |
|
3 |
Custom Units (PIN/POUT) per revolution |
|
4 |
counts 16-bit |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 4 |
|
Default Value |
1 |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.UNIT.PLINEAR | 0x5010 | 0x7 | USINT | - | - | RW | False |
| AXIS2.UNIT.PLINEAR | 0x5110 | 0x7 | USINT | - | - | RW | False |