AXIS#.UNIT.POUT
Description
AXIS#.UNIT.POUT is used with AXIS#.UNIT.PIN to set application specific units in AXIS#.UNIT.POUT. This parameter is used as follows in the drive unit conversion:
- For position, this parameter sets the units as Custom Units/rev.
- For velocity, this parameter sets the units as Custom Units/s.
- For acceleration/deceleration, this parameter sets the units as Custom Units/s2.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
User units. |
|
Range |
1 to 4,294,967,295 |
|
Default Value |
20 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.UNIT.POUT | 0x5010 | 0x2 | UDINT | - | - | RW | False |
| AXIS2.UNIT.POUT | 0x5110 | 0x2 | UDINT | - | - | RW | False |