AXIS#.UNIT.PROTARY
Description
AXIS#.UNIT.PROTARY sets the position units when the motor type (AXIS#.MOTOR.TYPE ) is rotary.
Value |
Units |
---|---|
0 |
counts |
1 |
rad |
2 |
degs |
3 |
Custom Units |
4 |
counts 16-bit |
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 to 4 |
Default Value |
0 |
Data Type |
Integer |
See Also |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.UNIT.PROTARY | 0x5010 | 0x5 | USINT | - | - | RW | False |
AXIS2.UNIT.PROTARY | 0x5110 | 0x5 | USINT | - | - | RW | False |