AXIS#.VL.LIMITP

Description

AXIS#.VL.LIMITP sets the velocity command positive limit.

If the input to the velocity loop is higher than AXIS#.VL.LIMITP, then the actual velocity command AXIS#.VL.CMD is limited by the value of AXIS#.VL.LIMITP.


  • ECCN 3A255 imposes special limitations on operating speed for induction motors. See ECCN 3A225 Limitations for Induction Motors.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: RPMClosed"Revolutions per minute" Is a unit of frequency of rotation: the number of full rotations completed in one minute around a fixed axis. It is used as a measure of rotational speed of a mechanical component, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value

15000 RPM

Depends on units. See Velocity Units for details.

Data Type

Float

See Also

AXIS#.VL.LIMITN , AXIS#.VL.CMD

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.VL.LIMITP 0x5011 0x6 UDINT - Velocity RW False
AXIS2.VL.LIMITP 0x5111 0x6 UDINT - Velocity RW False