AXIS#.WS.NUMLOOPS
Description
This parameter sets the maximum number of wake and shake repetitions. AXIS#.MOTOR.PHASE is calculated as mean value of all wake and shake repetitions.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
counts |
Range |
0 to 20 counts |
Default Value |
5 counts |
Data Type |
Integer |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.WS.NUMLOOPS | 0x5013 | 0x2 | USINT | - | - | RW | False |
AXIS2.WS.NUMLOOPS | 0x5113 | 0x2 | USINT | - | - | RW | False |