AXIS#.DISTO

Description

This timer starts when AXIS#.DIS is issued (regardless of the AXIS#.DIS origin). After this timeout elapses, the actual state of the drive is compared to the AXIS#.DISMODE setting. If the actual state does not match the AXIS#.DISMODE setting, a fault is reported and the hardware immediately executes the AXIS#.DISMODE setting (for instance, disable or activate dynamic brake). Setting AXIS#.DISTO to 0 will disable the timeout.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

ms

Range

0 to 120,000 ms

Default Value

1,000 ms

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.DISTO 0x5000 0x9 UDINT - - RW False
AXIS2.DISTO 0x5100 0x9 UDINT - - RW False