AXIS#.FAULT#
Description
This keyword can be used to extract individual faults from the axis specified.
The order of the faults are represented by the order of the faults thrown.
-
- Only the fault number is returned, no detail description is accompanied.
Examples
If there were two faults present on Axis1, they could be extracted using AXIS1.FAULT1 and AXIS1.FAULT2 seen below:
-->AXIS1.FAULT1
4312
-->AXIS1.FAULT2
4115
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read Only |
| Units | N/A |
| Range | N/A |
| Default Value | N/A |
| Data Type | Integer |
| See Also | AXIS#.FAULTS, DRV.FAULTS |
|
Stored in Non Volatile Memory |
No |
Variants Supported
Supported on all device types.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.FAULT1 | 0x5004 | 0x1 | UINT | - | - | RO | False |
| AXIS1.FAULT2 | 0x5004 | 0x2 | UINT | - | - | RO | False | |
| AXIS1.FAULT3 | 0x5004 | 0x3 | UINT | - | - | RO | False | |
| AXIS1.FAULT4 | 0x5004 | 0x4 | UINT | - | - | RO | False | |
| AXIS1.FAULT5 | 0x5004 | 0x5 | UINT | - | - | RO | False | |
| AXIS1.FAULT6 | 0x5004 | 0x6 | UINT | - | - | RO | False | |
| AXIS1.FAULT7 | 0x5004 | 0x7 | UINT | - | - | RO | False | |
| AXIS1.FAULT8 | 0x5004 | 0x8 | UINT | - | - | RO | False | |
| AXIS1.FAULT9 | 0x5004 | 0x9 | UINT | - | - | RO | False | |
| AXIS1.FAULT10 | 0x5004 | 0xA | UINT | - | - | RO | False | |
| AXIS2.FAULT1 | 0x5104 | 0x1 | UINT | - | - | RO | False | |
| AXIS2.FAULT2 | 0x5104 | 0x2 | UINT | - | - | RO | False | |
| AXIS2.FAULT3 | 0x5104 | 0x3 | UINT | - | - | RO | False | |
| AXIS2.FAULT4 | 0x5104 | 0x4 | UINT | - | - | RO | False | |
| AXIS2.FAULT5 | 0x5104 | 0x5 | UINT | - | - | RO | False | |
| AXIS2.FAULT6 | 0x5104 | 0x6 | UINT | - | - | RO | False | |
| AXIS2.FAULT7 | 0x5104 | 0x7 | UINT | - | - | RO | False | |
| AXIS2.FAULT8 | 0x5104 | 0x8 | UINT | - | - | RO | False | |
| AXIS2.FAULT9 | 0x5104 | 0x9 | UINT | - | - | RO | False | |
| AXIS2.FAULT10 | 0x5104 | 0xA | UINT | - | - | RO | False |