AXIS#.OPMODE

Description

AXIS#.OPMODE specifies the operation mode of the axis. You must also use AXIS#.CMDSOURCE to set the source of the command to the axis.

The operation mode values can be set as follows:

Mode

Description

0

Current (torqueClosedTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist) operation mode

1

Velocity operation mode

2

Position operation mode

AXIS#.OPMODE can be changed while the axis is enabled or disabled. If you are using the terminal to change the operation mode, it is recommended that you disable the axis before changing the operation mode. If you change the operation mode from the terminal while the axis is enabled, the system may experience a step change in demand.

Example

Set the source of the command to a TCP/IP channel and the desired operation mode to velocity:

-->AXIS1.CMDSOURCE 0

-->AXIS1.OPMODE 1

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 2

Default Value

0

Data Type

Integer

Stored in Non Volatile Memory

Yes

Gantry Mode

If the axis is in Gantry Mode (CMDSOURCE = 4), then this opmode setting has no effect until the CMDSOURCE is set to something other than 4 – Gantry.

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.OPMODE 0x5000 0x5 USINT - - RW False
AXIS2.OPMODE 0x5100 0x5 USINT - - RW False

Related Topics

Gantry Mode