DRV.CUSTOMIDENTIFIER
Description
Use DRV.CUSTOMIDENTIFIER to assign a unique string to a device. The string must use the following formatting rules:
- ASCII characters only
- 32 character max length
- No spaces in string
The string is displayed on the device overview screen and in the start page's device discovery table.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
N/A |
Default Value |
- |
Data Type |
String |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | DRV.CUSTOMIDENTIFIER | 0x3000 | 0x2 | STRING(32) | - | - | RW | False |