EEO#.PULSEWIDTH

Description

The pulse width of the pulses from the CW/CCW and step/dir modes,EEO#.MODE 1 or 2. In these modes this parameter also controls the width of the Z pulse. This parameter has no effect in the A quad B mode.


  • If the pulse width is too long it will effect the maximum speed of the output as the pulses will start to overlap. This formula is expressed as:
    MaxVelocity (rev/sec) <= 1/(Lines * PulseWidth_in_secs).

Examples

Code

This will set the pulse width to 8.16 us.

-->EEO1.PULSEWIDTH 8.16

Context

For more information see Encoder Emulation.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units us
Range 0.08 to 2621.40
Default Value 4.08
Data Type Float
See Also  
Stored in Non Volatile Memory Yes

Variants Supported

All variants are supported.