REC.NUMPOINTS

Description

REC.NUMPOINTS specifies the number of points (samples) to record.

Examples

Code

To record the maximum 10,000 samples:

-->REC.NUMPOINTS 10000

Context

For more information see Scope.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

1 to 10,000

Default Value

1,000

Data Type

Integer

See Also

REC.TRIG

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.