REC.RETRIEVE
Description
REC.RETRIEVE causes the drive to transfer all the recorded data to the communication channel. The data is encoded so that it can be interpreted by WorkBench.
Examples
Context
For more information see Scope.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
String |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.