USER.INT#
Description
Set of scratchpad variables users can use for read and write. Keywords can be selected as an Action Table source.
Examples
Usage
Code
Map to Modbus -->MODBUSModBus is a serial communications protocol and is now the most commonly available means of connecting industrial electronic devices. ModBus is often used to connect a supervisory computer with a remote terminal unit in supervisory control and data acquisition (SCADA) systems. Versions of the ModBus protocol exist for serial port and Ethernet (it is widely used with TCP/IP over Ethernet).MAP 40001 USER.INT2
Setup Action -->ACTION5.TASK 12 -->ACTION5.TASKID 1 -->ACTION5.SOURCE 23 -->ACTION5.SOURCEID 2 -->ACTION5.CONDITION 12 -->ACTION5.CONDITIONVALUE 20 -->ACTION5.ACTION 1
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-03-04-000 |
|
General Information
Type |
Read/Write |
Units | N/A |
Range |
-32768 to 32767 |
Default Value | 0 |
Data Type |
Integer |
See Also | ACTION#.SOURCE 23 |
Fieldbus Information
FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | - | 4100h | 1-10 | INT | - | - | RW | False |