VBUS.ACNOMINAL
Description
This keyword lets the user easily configure the operating voltage for a level other than the default of the drive.
-
-
The user can only de-rate a drive, and not operate it higher than the original voltage.
When changed, VBUS.ACNOMINAL will modify the inrush voltage settings as well as the Regen voltage configurations. It is important that VBUS.ACNOMINAL be set as accurately as possible to minimize voltage faults.
Examples
Code
If an HV drive (480V) was needed for bench testing at 120V, the user would do the following
VBUS.ACNOMINAL 120
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
VAC |
|
Range |
0 to Drive Rated Voltage |
|
Default Value |
Drive Rated Voltage |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.