VBUS.RMSLIMIT

Description

This parameter reads the limit of the bus capacitor AXIS#.LOAD. When the bus capacitor loads exceeds this limit, the drive generates fault F503.

Excessive bus capacitor load may indicate a disconnected main supply phase.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

VrmsClosedrms stands for root mean square (also known as the quadratic mean)

Range

N/A

Default Value

N/A

Data Type

Integer

See Also

N/A

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported

Related Topics

Regeneration