VBUS.UVMODE
Description
VBUS.UVMODE sets what happens when the under voltage, UV, condition is detected. An under voltage is triggered:
When VBUS.UVMODE = 0, an undervoltage fault is issued whenever the DC bus voltage, VBUS.VALUE, goes below the fault threshold, VBUS.UVFTHRESH.
When VBUS.UVMODE = 1, an undervoltage fault is issued whenever the DC bus voltage, VBUS.VALUE, goes below the fault threshold, VBUS.UVFTHRESH and the controller attempts to enable the drive (software or hardware enable).
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
1 |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
VBUS.UVMODE | 0x300A | 0x4 | USINT | - | - | RW | False |