AOUT.VALUEU
Description
AOUT.VALUEU reads/writes the analog output value when AOUT.MODE = 0 (analog output signal is determined by the user).
General Information
|
Type |
R/W Parameter |
|
Units |
V |
|
Range |
–10 to +10 V |
|
Default Value |
0 |
|
Data Type |
Float |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3470h/3 |
M_01-00-00-000 |
Related Topics