BODE.INJECTPOINT
Description
BODE.INJECTPOINT sets whether the excitation uses current or velocity excitation type.
|
BODE.INJECTPOINT |
Description |
|---|---|
|
0 |
None |
|
1 |
Current |
|
2 |
Velocity |
Example
Set BODE.INJECTPOINT to current:
-->BODE.INJECTPOINT 1
Get BODE.INJECTPOINT (already set to current):
-->BODE.INJECTPOINT 1
General Information
|
Type |
R/W Parameter |
|
Units |
N/A |
|
Range |
0 to 2 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
5016h/0 |
M_01-00-00-000 |
Related Topics
Using the Performance Servo Tuner
Using the Performance Servo Tuner: Advanced