CMPx.OUTMASK
Description
This keyword sets the binary output disable mask between the setpoint
Setpoint is the target value that an automatic control system, for example PID controller, will aim to reach and the drive's output pin. Note the internal setpoint state remains valid, only the external output is blocked.
Example
The following example sets an outmask to 7 (binary 111) to block setpoint states 0, 1, and 2 from asserting the drive output pin.
-->CMP0.OUTMASK 7
General Information
|
Type |
NV Parameter |
|
Units |
None |
|
Range |
0 to 255 |
|
Default Value |
0 (Inactive) |
|
Data Type |
Integer |
|
Start Version |
M_01-13-00-000 |
Hardware Supported
Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.
| AKD Type | Hardware Revision Supported |
|---|---|
| AKD | Revision D or higher |
| AKD PDMM | Revision DB or higher |
| AKD-T-IC |
Revision DA or higher |
Variants Supported
*In SynqNet
SynqNet is a digital machine control network. Built on the 100BT physical layer, SynqNet provides a synchronous real-time connection between motion controllers, servo drives, stepper drives, I/O modules, and custom devices, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
| Fieldbus |
Index/Subindex | Object Start Version | |
|---|---|---|---|
| 5394h/0 |
CMP0.OUTMASK |
M_01-13-00-000 | |
| 539Bh/0 |
CMP1.OUTMASK |
||
Related Topics