COGCOMP.RANGELOW
Description
This parameter stores the position of the lower end of the range where cogging compensation is active on a linear axis. On rotary axis, it stores the position of the lower end of the range when the parameter is unequal to 0.
When the value is changed while compensation values are configured, the compensation values will be redistributed over the new range, which will most likely lead to incorrect compensation.
Before starting COGCOMP.TEACH on a linear axis, the value in COGCOMP.RANGELOW has to be smaller than COGCOMP.RANGEHIGH.
General Information
This content is not applicable to KAS.
Type |
NV Parameter |
Units |
Position units |
Range |
-9,223,372,036,854,774 [counts] to 9,223,372,036,854,774 [counts] or equivalent in position units |
Default Value |
0 |
Data Type |
Float |
Start Version |
M_01-14-06-001 |
Fieldbus![]() |
Index/Subindex | Object Start Version |
---|---|---|
5418h/0 |
M_01-14-06-001 |