DOUT.RELAYMODE
Description
DOUT.RELAYMODE indicates the faults relay mode as follows:
If DOUT.RELAYMODE= 0 and faults exist, then the relay is open.
If DOUT.RELAYMODE= 0 and faults do not exist, then the relay is closed.
If DOUT.RELAYMODE = 1 and the drive is disabled, then the relay is open.
If DOUT.RELAYMODE = 1 and the drive is enabled, then the relay is closed.
General Information
|
Type |
R/W Parameter |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
5060h/0 |
M_01-00-00-000 |
Related Topics