DRV.CUSTOMIDENTIFIER
Description
Use DRV.CUSTOMIDENTIFIER to assign a unique string to a device. The string must use the following formatting rules:
- ASCII characters only
- 32 character max length
- No spaces in string
The string is displayed on the device overview screen and in the start page's device discovery table.
General Information
|
Type |
NV Parameter |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
String |
|
Start Version |
M_01-12-05-000 |
| Fieldbus |
Index/Subindex | Object Start Version |
|---|---|---|
|
2032h/0 |
M_01-12-05-000 |
Related Topics