DRV.IZERO
Description
This parameter sets the current that is used during the DRV.ZERO procedure.
General Information
|
Type |
NV Parameter |
|
Units |
Arms |
|
Range |
Drive peak current to 0 Arms |
|
Default Value |
0 Arms |
|
Data Type |
Float |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
5085h/0 |
M_01-00-00-000 |
Related Topics