DRV.REBOOT

Description

This parameter performs a software reboot when the following command is issued in the WorkBench terminal:

DRV.REBOOT 0xAABBCCDD

WorkBench will disconnect from the AKD when the reboot command is executed. The AKD can be reconnected to WorkBench approximately one minute after the reboot command is issued. The parameters stored in non-volatile memory will be restored to the AKD once rebooted.

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

Integer

Start Version

M_01-13-08-000