DRV.SETUPREQLIST

Description

This parameter returns the list of parameters that must be set before the drive can be enabled and also whether or not each one of those parameters is set. This list of parameters will vary depending on the value MOTOR.TYPE. The drive can only be enabled when all commands have a value of 0.

Example

-->DRV.SETUPREQLIST

ILClosed"Instruction list" This is a low-level language and resembles assembly.KP 0

MOTOR.ICONT 0

MOTOR.IPEAK 0

MOTOR.POLES 0

-->

General Information

Type

R/O Parameters

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-00-00-000

Related Topics

DRV.SETUPREQBITS , MOTOR.AUTOSET