FAULTx.ACTION
Description
This Parameter determines the action the drive should take when Fault 130, 131, 132, 134, 139, 451, or 702 occurs.
| Parameter Value | Drive Action |
|---|---|
| 0 | Disable Ampllifier |
| 1 | Ignore (fault will not be reported) |
General Information
|
Type |
R/W |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Start Version |
M_01-04-16-000 |
| Fieldbus |
Index/Subindex | Object Start Version | |
|---|---|---|---|
| 5259h/0 | FAULT130.ACTION | M_01-04-16-000 | |
| 525Ah/0 | FAULT131.ACTION | ||
| 525Bh/0 | FAULT132.ACTION | ||
| 525Ch/0 | FAULT134.ACTION | ||
|
5267h/0 |
FAULT451.ACTION | ||
| 525Dh/0 | FAULT702.ACTION | ||