IL.FOLDFTHRESHU
Description
IL
"Instruction list"
This is a low-level language and resembles assembly.FOLDFTHRESHU is the fault level of the current foldback algorithm. The value of IL.FOLDFTHRESH is the minimum of DRV.IPEAK
, MOTOR.IPEAK
, and IL.FOLDFTHRESHU.
General Information
|
Type |
NV Parameter |
|
Units |
Arms |
|
Range |
0 to 500 Arms |
|
Default Value |
Drive peak current (DRV.IPEAK) |
|
Data Type |
Float |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3421h/0 |
M_01-00-00-000 |
Related Topics
1 Current Loop