IL.KPDRATIO
Description
This parameter sets the proportional gain of the PI-loop, which controls the d-component of the current.
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 2 |
|
Default Value |
1 |
|
Data Type |
Float |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3596h/0 |
M_01-00-00-000 |
Related Topics
1 Current Loop