IL.MFOLDR
Description
IL
"Instruction list"
This is a low-level language and resembles assembly.MFOLDR sets the recovery time for the motor foldback algorithm. If 0 current is applied for at least the recovery time duration, it is possible to apply motor peak current for the duration of IL.MFOLDD time.
The IL.MFOLDR value is automatically calculated from other foldback parameters.
General Information
|
Type |
R/O Parameter |
|
Units |
s |
|
Range |
0.1 to 65,535 s |
|
Default Value |
Calculated from other foldback parameters. |
|
Data Type |
Float |
|
See Also |
Foldback |
|
Start Version |
M_01-00-00-000 |
Related Topics
1 Current Loop