IL.VLIMIT
Description
IL
"Instruction list"
This is a low-level language and resembles assembly.VLIMIT sets the velocity limit for operation in torque
Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist mode.
When set to a non-zero value, the current supplied to the motor will be limited to prevent the drive from accelerating beyond -IL.VLIMIT / IL.VLIMIT.
General Information
|
Type |
NV Parameter |
|
Units |
Depends on UNIT.VROTARY or UNIT.VLINEAR Rotary: rpm, rps, deg/s, custom units/s, rad/s Linear: counts/s, mm/s, µm/s |
|
Range |
Rotary: 0.000 to 15,000.000 rpm 0.000 to 250.000 rps 0.000 to 90,000.000 deg/s 0.000 to 1,250.000 custom units/s 0.000 to 1570.796 rad/s Linear: 0.000 to 1,073,741,824,000.000 counts/s 0.000 to 250.000*MOTOR.PITCH mm/sec 0.000 to 250,000.000*MOTOR.PITCH µm/s |
|
Default Value |
Rotary: 0.000 rpm 0.000 rps 0.000 deg/s 0.000 custom units/s 0.000 rad/s Linear: 0.000 counts/s 0.000*MOTOR.PITCH mm/sec 0.000 *MOTOR.PITCH µm/sec |
|
Data Type |
Float |
|
Start Version |
M_01-14-04-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
207Fh/0 |
M_01-14-04-000 |
Related Topics
1 Current Loop