MOTOR.ICONT
Description
This parameter is used to configure the motor continuous current.
-
- This parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET=1.
General Information
|
Type |
NV Parameter |
|
Units |
A |
|
Range |
0.1 to 500 A |
|
Default Value |
1.0 A |
|
Data Type |
Float |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
358Eh/0 |
M_01-00-00-000 |
Related Topics