MOTOR.PHASE
Description
This parameter sets the motor phase.
-
-
If MOTOR.AUTOSET = 1 and FB1.MEMVER > 0.01, this parameter will be automatically configured for Kollmorgen motors.
-
- When loading a parameter file to a new device, if MOTOR.AUTOSET = 0 then motor parameters should be checked to make sure they are properly configured for the motor on the new device.
General Information
|
Type |
NV Parameter |
|
Units |
Electrical degrees |
|
Range |
0 to 360° |
|
Default Value |
0° |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
359Ch/0 |
M_01-00-00-000 |
Related Topics