MOTOR.R
Description
MOTOR.R sets the stator winding resistance phase-to-phase in ohms.
-
- This parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET=1.
General Information
|
Type |
NV Parameter |
|
Units |
Ω |
|
Range |
0.001 to 650 Ω |
|
Default Value |
10 Ω |
|
Data Type |
Float |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3456h/0 |
M_01-00-00-000 |
Related Topics