PL.FBSOURCE
Description
This parameter determines the feedback source that the position loop uses. A value of 0 for this parameter selects the primary feedback, a value of 1 selects the secondary feedback. If you use the secondary feedback as the source for the position loop, then FB2.MODE mode should be set as 0 (A/B signals). A/B signals are the only supported feedback type as secondary feedback into the position loop. Other settings for FB2.MODE are intended as pulse inputs or a gearing command when PL.FBSOURCE remains 0.
| 0 |
Primary Feedback connected to X10. |
| 1 | Secondary Feedback (DRV.HANDWHEEL) connected to X7 or X9. |
| 2 | Tertiary Feedback connected to X9 (only supported with AKD-x-xxxxx-NBxx-xxxx). |
General Information
|
Type |
NV Parameter |
|
Units |
N/A |
|
Range |
Range will differ depending on drive model. |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
5128h/0 |
M_01-00-00-000 |
Related Topics